Industrial Robots
- What is the payload amount for the OVR series 4-Axis Articulated Robot?
- What are the Voltage specifications for the MRCU controller ?
- Can you reset the Alarms on the MRCU ?
- Are there any alarm function that the OVR systems have ?
- Can you check the Alarm History on the MRCU controller ?
- Is the MRCU controller equipped with a function to generate information output before an alarm ca be generated?
- Is there a information that can be stored on the MRCU and then shared via the I/O
- What do the LEDs on the MRCU controllers mean?
- What is the main power supply current capacity for the MRCU controller?
- What is the Current Capacity for Control Power Supply on the MRCU ?
- Do you offer a programming software for the OVR Robots?
- What type of end effectors does Oriental Motor offer for OVR Robots?
- What is the payload amount for the 5-Axis Articulated Robot?
- What is the payload amount for the 6-Axis Articulated Robot?
- What is the payload amount for the 3-Axis SCARA Robot?
- What is the payload amount for the 3-Axis Cartesian Robot?
- Do you offer industrial robots?
- What are the significant specs for the OVR Series Cartesian 3-Axis robot ?
- What are the significant specs for the OVR series SCARA robot ?
- What are the significant specs for the 4-Axis OVR series robot ?
- What are the significant specs for the 5-axis OVR series robot ?
- What are the significant specs for the 6-Axis OVR series robot ?
- What motion commands are supported in the MRC Studio software?
- What are some application we can use the OVR series robots systems in?
- What happens when you use the "FREE" control on the MRC studio?
- What are the control methods of the MRC01 Robot Controller ?
- Can I use a third party end effector with Oriental Motor OVR series Robot?
- Why can I not see the Simulator Software Program MRCXT file open ?
- How many control commands are there in the MRC Studio software?
- Electric Robotic arms vs Pneumatic Robotic Arms
- Can you mount the OVR on a vertical wall?
- What are the Installation Location Recommendation for the OVR and MRC Products?