---
title: Controllers / Drivers | FAQ / KnowledgeBase
description: Controllers / Drivers
---

[Skip to content](https://faq.orientalmotor.com/controllers-drivers#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/)
2. [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers)

# Controllers / Drivers

- [What kind of PLC communication protocols does Oriental Motor offer?](https://faq.orientalmotor.com/what-kind-of-plc-communication-protocols-does-oriental-motor-offer)
- [For the AZ Series with built-in positioning function, is it possible to use FA network control and direct input/output at the same time?](https://faq.orientalmotor.com/for-the-az-series-with-built-in-positioning-function-is-it-possible-to-use-fa-network-control-and-direct-input/output-at-the-same-time)
- [How many milliseconds is the communication cycle of the AZ Series EtherNet/IP compatible driver?](https://faq.orientalmotor.com/how-many-milliseconds-is-the-communication-cycle-of-the-az-series-ethernet/ip-compatible-driver)
- [I am using the AZ series EtherNet/IP compatible driver. The fixed I/O signal EXE-ERR is ON. What kind of signal is EXE-ERR?](https://faq.orientalmotor.com/i-am-using-the-az-series-ethernet/ip-compatible-driver.-the-fixed-i/o-signal-exe-err-is-on.-what-kind-of-signal-is-exe-err)
- [Can I use 1 EMC filter in the input power supply connection for multiple drivers/controllers?](https://faq.orientalmotor.com/can-i-use-1-emc-filter-in-the-input-power-supply-connection-for-multiple-drivers/controllers)
- [Can I use the power cutoff function of the AZ series as an emergency stop function in the event of an abnormality?](https://faq.orientalmotor.com/can-i-use-the-power-cutoff-function-of-the-az-series-as-an-emergency-stop-function-in-the-event-of-an-abnormality)

See less ▼

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors)
- [Variable Speed / Brushless DC Motors](https://faq.orientalmotor.com/variable-speed-brushless-dc-motors)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers)
- [Software](https://faq.orientalmotor.com/software)
- [Networking](https://faq.orientalmotor.com/networking)
- [General](https://faq.orientalmotor.com/general)
- [Servo](https://faq.orientalmotor.com/servo)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom)

- Home
- Products
- Pricing
- Blog
- Company

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.