---
title: What are the Installation Location Recommendation for the OVR and MRC Products?
description: FAQ / KnowledgeBase
---

[Skip to content](https://faq.orientalmotor.com/what-are-the-installation-location-recommendation-for-the-ovr-and-mrc-products#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/?hsLang=en)
2. [Industrial Robots](https://faq.orientalmotor.com/industrial-robots?hsLang=en)

# What are the Installation Location Recommendation for the OVR and MRC Products?

## Installation Location and Connection

The products are designed and manufactured to be incorporated into general  
industrial equipment. Install it in a well-ventilated location that provides easy access for inspection.  
The location must also satisfy the following conditions:

- Inside an enclosure installed indoors (provide ventilation holes)
- Operating ambient temperature: 0 to +40 °C \[+32 to 104 °F\] (non-freezing)  
  Operating ambient humidity: 85 % or less (non-condensing)  
  Area free of explosive atmosphere, toxic gas (such as sulfuric gas), or liquid  
  Area not exposed to direct sun  
  Area free of excessive amount of dust, iron particles, or the like  
  Area not subject to splashing water (rain, water droplets), oil (oil droplets), or other liquids  
  Area free of excessive salt  
  Area not subject to continuous vibration or excessive shocks  
  Area free of excessive electromagnetic noise (from welders, power equipment, etc.)  
  Area free of radioactive materials, magnetic fields, or vacuum  
  Up to 1,000 m (3,300 ft.) above sea level

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo?hsLang=en)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors?hsLang=en)
- [Variable Speed Motors](https://faq.orientalmotor.com/variable-speed-motors?hsLang=en)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators?hsLang=en)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors?hsLang=en)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots?hsLang=en)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans?hsLang=en)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers?hsLang=en)
- [Software](https://faq.orientalmotor.com/software?hsLang=en)
- [Networking](https://faq.orientalmotor.com/networking?hsLang=en)
- [General](https://faq.orientalmotor.com/general?hsLang=en)
- [Servo](https://faq.orientalmotor.com/servo?hsLang=en)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom?hsLang=en)

- Home
- Products
- Pricing
- Blog
- Company

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.