Skip to content
  • There are no suggestions because the search field is empty.

What are the Voltage specifications for the MRCU controller ?

The power supply input voltage specifications include the rated voltage and the allowable operating voltage. 

 

Rated Voltage  

Allowable Operating Voltage  

Main Power Supply  

24 VDC±5 %  

48 VDC±5 % 

24 VDC input: 20 to 32 VDC (22.8 to 32 VDC) 48 VDC input: 40 to 55 VDC 

Control Power Supply  

24 VDC±5 % 

20 to 27.6 VDC( 22.8 to 27.6 VDC) 

*The value in parentheses ( ) is the value when the electromagnetic brake motor is connected. 

Note Do not apply 48 VDC to the control power supply. Doing so may result in damage to the controller.