How Does one set up the Robot on the MRC Studio?
Setting up Robot on the MRC studio .
Set the information of the robot with the MRC Studio software.
1. Start the MRC Studio software.
2. Click [COM port] to select “MRC01.”
3. Click [Setup] on the start screen.
4. Set the robot type and the mechanism information according to the instructions on the screen.
*To change the robot type, perform the setup again from the start screen. Except for the robot type, you can change using [Re-setup] under the [Maintenance] menu even after the setup is completed*