Variable Speed Motors
- What is the difference between "velocity fluctuation rate" and "flutter characteristics"?
- The alarm LED on my MSC series speed control motor unit is flashing 9 times. What could be the cause?
- What applications are BLDC motors best used for?
- What is the feedback system used for speed control on the DSC and US2 AC speed control series?
- I am using the DSC series and an alarm code beginning with AL is displayed on the front panel of the speed controller. What is the meaning of this alarm code?
- Can I set acceleration/deceleration on the BMU series?
- I connected the external operation signal FWD input/REV input to the BMU series and turned the input ON, but it doesn't work. Why doesn't it work?
- Is the output voltage of the tachogenerator wire of the AC speed control motor (6 to 90W) DC or AC? Also, what is the voltage level?
- I am using the BMU series and the message "AL30" is displayed on the front panel of the driver. What does AL30 mean?
- The alarm LED on the MSC series speed control motor unit is flashing twice. What is the cause?