Servo
- I'm using a servo motor, and an overvoltage protection alarm is being triggered. When does this alarm occur? Also, how can I resolve this issue?
- When using the NX series in torque control mode, how much error is there between the command torque value and the actual output torque?
- What happens if acceleration/deceleration is not controlled with a servo motor?
- What is the allowable load moment of inertia?
- What kind of earth leakage breaker should I use?