Skip to content
  • There are no suggestions because the search field is empty.

How do you set up the MRC Studio Software? 

Oriental motor offers a Free MRC studio software for it Robot product lines. 

Set the information of the robot with the MRC Studio software.
1. Start the MRC Studio software.
2. Click [Communication port] to select [MRCU].
3. Click [Setup] on the start screen.
4. On the “Introduction” screen, check “The connection was removed.” and proceed to the next
screen.

5. Then follow the on-screen instructions to set up.

Tip
To change the robot type, perform the setup again from the start screen. Except for the robot type,
using [Re-setup] in the [Maintenance] menu can change even after the setup is completed.