Industrial Robots
- How do I Check for theTCP position limit of my OVR robot vias the MRC studio software .
- How do I check the origin of my OVR robot Via the MRC Studio software ?
- How do I set the position limit on the MRC Studio Software
- What is the Definition of right-handed system / left-handed systems in SCARA and 6 Axis robots?
- What the Coordinate system the OVR robots can work with ?
- How many degrees of freedoms are present for each robot type ?
- Is the MRC01 and the MRC01-C the same controller ?
- What are the I/O signals cables that are offered for the MRCU controllers ?
- What connection cables / flexible connection cables are offered for the OVR motors ?
- What is the power supply cable for the MRCU Robot controller and there pin out ?
- Does the MRCU controller need any maintenance ?
- How do you set up the MRC Studio Software?
- For the MRCU and OVR robots, are there any noise suppression tips we can use ?
- For the MRCU and OVR robots are there any prevention of noise propagation tips we can use ?
- What is the main power supply current capacity for the MRCU controller?
- What do the LEDs on the MRCU controllers mean?
- What is the Current Capacity for Control Power Supply on the MRCU ?
- Is there a information that can be stored on the MRCU and then shared via the I/O
- Is the MRCU controller equipped with a function to generate information output before an alarm ca be generated?
- Can you check the Alarm History on the MRCU controller ?
- Can you reset the Alarms on the MRCU ?
- What are the Voltage specifications for the MRCU controller ?
- Are there any alarm function that the OVR systems have ?
- What is the payload amount for the OVR series 4-Axis Articulated Robot?
- Do you offer a programming software for the OVR Robots?
- What type of end effectors does Oriental Motor offer for OVR Robots?
- What is the payload amount for the 5-Axis Articulated Robot?
- What is the payload amount for the 6-Axis Articulated Robot?
- What is the payload amount for the 3-Axis SCARA Robot?
- What is the payload amount for the 3-Axis Cartesian Robot?
- Do you offer industrial robots?
- What are the significant specs for the OVR Series Cartesian 3-Axis robot ?
- What are the significant specs for the OVR series SCARA robot ?
- What are the significant specs for the 4-Axis OVR series robot ?
- What are the significant specs for the 5-axis OVR series robot ?
- What are the significant specs for the 6-Axis OVR series robot ?
- What motion commands are supported in the MRC Studio software?
- What are some application we can use the OVR series robots systems in?
- What happens when you use the "FREE" control on the MRC studio?
- What are the control methods of the MRC01 Robot Controller ?
- Can I use a third party end effector with Oriental Motor OVR series Robot?
- Why can I not see the Simulator Software Program MRCXT file open ?
- How many control commands are there in the MRC Studio software?
- Electric Robotic arms vs Pneumatic Robotic Arms
- Can you mount the OVR on a vertical wall?
- What are the Installation Location Recommendation for the OVR and MRC Products?
- For the MRCU is there any concerns for Surge Suppressors ?
- How Does one set up the Robot on the MRC Studio?
- How do I set the Origin of my robot Through the MRC Software ?