---
title: Networking | FAQ / KnowledgeBase
description: Networking
---

[Skip to content](https://faq.orientalmotor.com/networking#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/)
2. [Networking](https://faq.orientalmotor.com/networking)

# Networking

- [Do you offer PLC setup files/manuals?](https://faq.orientalmotor.com/do-you-offer-plc-setup-files/manuals)
- [I'm rewriting parameters through communication (CC-Link network converter NETC01-CC to AZ), but when I turn the power back on, the parameters I thought I had changed disappear. Why is that?](https://faq.orientalmotor.com/im-using-the-az-series-with-the-network-converter-netc01-cc-to-control-it-through-cc-link-communication.-im-rewriting-parameters-through-communication-but-when-i-1727211379238)
- [I am using Modbus RTU control on the AR series with built-in positioning function. After turning the START input bit ON and running the controller, do I need to turn it OFF?](https://faq.orientalmotor.com/i-am-using-modbus-rtu-control-on-the-ar-series-with-built-in-positioning-function.-after-turning-the-start-input-bit-on-and-running-the-controller-do-i-need-to-turn-it-off)
- [When data is written using the αSTEP AZ Drivers with Ethernet/IP communication, my changes are not saved in the drive and reverted back to the previous settings after a power cycle. How do I fix this?](https://faq.orientalmotor.com/i-am-using-the-ethernet/ip-compatible-driver-for-the-az-series.-i-wrote-operation-data-via-communication-but-when-i-turned-the-power-back-on-the-data-reverted-to-1750692059550)
- [Do you offer add on instructions (AOIs) for your PLC based drivers?](https://faq.orientalmotor.com/do-you-offer-add-on-instructions-aois-for-your-plc-based-drivers)
- [Do you offer any drivers that can be used with microcontrollers?](https://faq.orientalmotor.com/do-you-offer-any-drivers-that-can-be-used-with-microcontrollers)

See less ▼

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors)
- [Variable Speed Motors](https://faq.orientalmotor.com/variable-speed-motors)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers)
- [Software](https://faq.orientalmotor.com/software)
- [Networking](https://faq.orientalmotor.com/networking)
- [General](https://faq.orientalmotor.com/general)
- [Servo](https://faq.orientalmotor.com/servo)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom)

- Home
- Products
- Pricing
- Blog
- Company

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.