---
title: What are the significant specs for the 4-Axis OVR series robot ?
description: The OVR Series Articulated 4-axis small horizontal transport robot features a simple mechanism that can be easily controlled and constructed cost-effectively
---

[Skip to content](https://faq.orientalmotor.com/what-are-the-significant-specs-for-the-4-axis-ovr-robot#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/?hsLang=en)
2. [Industrial Robots](https://faq.orientalmotor.com/industrial-robots?hsLang=en)

# What are the significant specs for the 4-Axis OVR series robot ?

The [OVR Series Articulated 4-axis](https://catalog.orientalmotor.com/viewitems/industrial-robots-articulated-robots/ovr-series-4-axis-articulated-robots?_gl=1*1mz98hu*_gcl_au*MjAxODc1Mzc4NC4xNzQ4Mzg1NjIw*_ga*NTI1NDg1NTQ1LjE3MDY2MzU2NzM.*_ga_VV8FQHSH1R*czE3NTEzMTIxNDgkbzk0MiRnMSR0MTc1MTMyMDU0NyRqNTIkbDAkaDY5MzA2OTMzMg..) small horizontal transport robot features a simple mechanism that can be easily controlled and constructed cost-effectively

- Parallel link mechanism
- Transportable mas
- ![ovr4068k5-v-img-200px](https://faq.orientalmotor.com/hs-fs/hubfs/ovr4068k5-v-img-200px.jpg?width=200&height=200&name=ovr4068k5-v-img-200px.jpg)s 5 kg
- Horizontal reach 480 / 680 / 880 mm
- Vertical reach 450 / 550 / 650 mm
- Rotational Wrist addition possible
- Robot weight 16.5 kg / 17.4kg / 26.9 kg
- Repetitive Positioning Accuracy ±0.05 mm
- Standard Cycle Time 0.7 sec

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo?hsLang=en)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors?hsLang=en)
- [Variable Speed Motors](https://faq.orientalmotor.com/variable-speed-motors?hsLang=en)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators?hsLang=en)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors?hsLang=en)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots?hsLang=en)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans?hsLang=en)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers?hsLang=en)
- [Software](https://faq.orientalmotor.com/software?hsLang=en)
- [Networking](https://faq.orientalmotor.com/networking?hsLang=en)
- [General](https://faq.orientalmotor.com/general?hsLang=en)
- [Servo](https://faq.orientalmotor.com/servo?hsLang=en)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom?hsLang=en)

- Home
- Products
- Pricing
- Blog
- Company

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.