---
title: αSTEP Step-Servo | FAQ / KnowledgeBase
description: αSTEP Step-Servo
---

[Skip to content](https://faq.orientalmotor.com/αstep-step-servo#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/)
2. [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo)

# αSTEP Step-Servo

- [What is the replacement for the ARD-AD and BAT01A?](https://faq.orientalmotor.com/what-is-the-replacement-for-the-ard-ad-and-bat01a)
- [What type of encoder is used on the AZ series step-servo hybrid motors?](https://faq.orientalmotor.com/what-type-of-encoder-is-used-on-the-az-series)
- [For the AR/AZ series pulse train input type, how many pulses are output per rotation of the motor output shaft for the A-phase pulse output (ASG) and B-phase pulse output (BSG)?](https://faq.orientalmotor.com/for-the-ar/az-series-pulse-train-input-type-how-many-pulses-are-output-per-rotation-of-the-motor-output-shaft-for-the-a-phase-pulse-output-asg-and-b-phase-pulse-output-bsg)
- [How much deviation is required to output an excessive position deviation alarm?](https://faq.orientalmotor.com/how-much-deviation-is-required-to-output-an-excessive-position-deviation-alarm)
- [The rotation speed units in the catalog are listed as two types, \[Hz\] and \[r/min\]. What is the difference between them?](https://faq.orientalmotor.com/the-rotation-speed-units-in-the-catalog-are-listed-as-two-types-hz-and-r/min.-what-is-the-difference-between-them)
- [For the AR series pulse train input type, what are the conditions for the END output to turn ON (the positioning complete signal to be output)?](https://faq.orientalmotor.com/for-the-ar-series-pulse-train-input-type-what-are-the-conditions-for-the-end-output-to-turn-on-the-positioning-complete-signal-to-be-output)
- [I am using an αSTEP AZ EtherNet/IP compatible driver. Is direct I/O wiring required?](https://faq.orientalmotor.com/i-am-using-an-ethernet/ip-compatible-driver-for-the-az-series.-is-direct-i/o-cn7-wiring-required)
- [I want to use the AZ series only on positive coordinates. How do I set this?](https://faq.orientalmotor.com/i-want-to-use-the-az-series-only-on-positive-coordinates.-how-do-i-set-this)
- [Do you offer vacuum rated motors?](https://faq.orientalmotor.com/do-you-offer-vacuum-rated-motors)
- [Does the AZ series EtherNet/IP compatible driver support explicit communication?](https://faq.orientalmotor.com/does-the-az-series-ethernet/ip-compatible-driver-support-explicit-communication)
- [I want to use the AZ series only on positive coordinates. Please tell me how to set it up.](https://faq.orientalmotor.com/i-want-to-use-the-az-series-only-on-positive-coordinates.-please-tell-me-how-to-set-it-up)
- [When using the AZ series or AR series with an electromagnetic brake for up and down movement, is it okay to release the electromagnetic brake at the same time as turning on the power?](https://faq.orientalmotor.com/when-using-the-az-series-or-ar-series-with-an-electromagnetic-brake-for-up-and-down-movement-is-it-okay-to-release-the-electromagnetic-brake-at-the-same-time-as-turning-on-the-power-)

See less ▼

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors)
- [Variable Speed Motors](https://faq.orientalmotor.com/variable-speed-motors)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers)
- [Software](https://faq.orientalmotor.com/software)
- [Networking](https://faq.orientalmotor.com/networking)
- [General](https://faq.orientalmotor.com/general)
- [Servo](https://faq.orientalmotor.com/servo)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom)

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.