Skip to content
  • There are no suggestions because the search field is empty.

Can you check the Alarm History on the MRCU controller ?

Up to 10 generated alarm items are stored in non-volatile memory in order from most recent to oldest. The stored alarm history can be read or cleared if any of the following operations is performed.

Yes you can read the alarm history on the MRCU via the following methods ; 

  • Read the alarm history with the monitor command via communication.
  • Clear the alarm history with the maintenance command via communication.
  • Read or clear the alarm history using the MRC Studio software.