---
title: What is the main power supply current capacity for the MRCU controller?
description: MRCU Current Capacity for Main Power Supply
---

[Skip to content](https://faq.orientalmotor.com/what-are-the-current-capacities-for-the-main-power-supply-#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/?hsLang=en)
2. [Industrial Robots](https://faq.orientalmotor.com/industrial-robots?hsLang=en)

# What is the main power supply current capacity for the MRCU controller?

## The current capacity for the main power supply varies depending on the OVR and AZ product combined. Refer to the table below.

Small Robot OVR series 

| Model | Power Supply Current Capacity |
| --- | --- |
| OVR3041K3-H | 6.7 A or more |
| OVR3AL030030Z10K-C OVR3AR030030Z10K-C | 6.9 A or more |
| OVR4048K5-V OVR4068K5-V OVR4088K5-V | 12.5 A or more |
| OVR5035K1-V | 14.3 A or more |
| OVR6048K1-V | 15.3 A or more |

Stepper Motors AZ series

| Model | Power Supply Current Capacity |
| --- | --- |
| AZM14 | 0.4 A or more |
| AZM15 | 0.5 A or more |
| AZM24, AZM26 | 1.4 A or more |
| AZM46 | 1.6 A or more |
| AZM48 | 2.1 A or more |
| AZM66 | 3.7 A or more |
| AZM69 | 3.5 A or more |

Motorized Actuator - EAC Series\*,EAS Series\*,EZS Series

| Model | Power Supply Current Capacity |
| --- | --- |
| AZM24 | 1.4 A or more |
| AZM46 | 1.6 A or more |
| AZM66 | 3.7 A or more |

Motorized Actuator - DGII Series 

| Model | Power Supply Current Capacity |
| --- | --- |
| DGM60 | 1.4 A or more |
| DGB85 | 1.6 A or more |
| DGB130 | 3.7 A or more |
| DGM85 | 1.6 A or more |
| DGM130 | 3.7 A or more |

Motorized Actuator - DR Series 

| Model | Power Supply Current Capacity |
| --- | --- |
| DR20 | 0.4 A or more |
| DR28 | 1.3 A or more |

Motorized Actuator - DRS2 Series 

| Model | Power Supply Current Capacity |
| --- | --- |
| DRSM42 | 1.5 A or more |
| DRSM60 | 2.6 A or more |

Motorized Actuator - EH Series 

| Model | Power Supply Current Capacity |
| --- | --- |
| EH3 | 0.4 A or more |
| EH4 | 1.4 A or more |

Motorized Actuator - L Series 

| Model | Power Supply Current Capacity |
| --- | --- |
| LM2, LM4 | 3.7 A or more |

 

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo?hsLang=en)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors?hsLang=en)
- [Variable Speed Motors](https://faq.orientalmotor.com/variable-speed-motors?hsLang=en)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators?hsLang=en)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors?hsLang=en)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots?hsLang=en)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans?hsLang=en)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers?hsLang=en)
- [Software](https://faq.orientalmotor.com/software?hsLang=en)
- [Networking](https://faq.orientalmotor.com/networking?hsLang=en)
- [General](https://faq.orientalmotor.com/general?hsLang=en)
- [Servo](https://faq.orientalmotor.com/servo?hsLang=en)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom?hsLang=en)

- Home
- Products
- Pricing
- Blog
- Company

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.