Skip to content
  • There are no suggestions because the search field is empty.

Can you reset the Alarms on the MRCU ?

Alarm Reset can be achieved via maintenance commands or the FREE MRC studio software 

Before resetting an alarm, always correct the cause of the alarm and ensure safety, and perform any of the reset operations listed below.
  •  Turn the ALM-RST input from OFF to ON. (It is enabled at the ON edge. )
  • Execute the alarm reset by the maintenance command via communication.
  • Execute the alarm reset using the MRC Studio software.
  • Turn the power off and on again.

Note:

Some alarms can only be reset by turning the power off and on again.