AC Gearmotors
- I have a motor with a non-excitation-operated electromagnetic brake, and I want to switch the power to both the motor and the electromagnetic brake on and off using a single contact. Are there any problems with this?
- Can motors and fans with a power supply voltage of 100V AC be used with an AC110V power supply?
- What applications are ACSC motors best used for?
- Is the surge suppression CR circuit "EPCR1201-2" shown in the wiring diagram of the circuit product necessary?
- The AC motor is very hot. Is this normal?
- I want to connect a pulley directly to the output shaft of the gearhead and transmit power with a belt, but if the radial load becomes large. What should I do?
- I want to run an induction motor in forward and reverse. How should I wire it?
- Why do single-phase AC motors need capacitors?
- Can I use capacitors other than the one that comes with the AC motor?
- What is the amount of overrun for an AC motor?
- What is the backlash of the gearhead that is combined with the AC motor?
- What is the IP Rating for the SMK Series?
- The catalog shows rated torque and permissible torque, but what is the difference?
- I have the TM series CW (CCW) input turned ON, but the motor does not move. The POWER LED is lit, so power is being input. What is the reason it does not move?
- Can a single-phase motor be driven by an inverter?
- When using a gearhead with an induction motor, what should I refer to when determining the rotation speed?
- Can I use a gearhead to reduce the motor rotation speed to 1/18,000?