What is the backlash of the gearhead that is combined with the AC motor?

Backlash is 1° to 2° (reference value). Backlash will vary slightly depending on the size of the gearhead, reduction ratio, and differences in the gear cutting shape for each type, but it will generally be within this range.