Skip to content
  • There are no suggestions because the search field is empty.

The catalog shows rated torque and permissible torque, but what is the difference?

The difference between rated torque and permissible torque is as follows:

Rated Torque
This refers to the torque when a motor continuously produces rated power at rated voltage and rated frequency.



Permissible Torque
This refers to the maximum (upper limit) torque that can be used when operating a motor.
The upper limit is determined by factors such as the strength of the gearhead and the rated torque of the motor.