Can I use a gearhead to reduce the motor rotation speed to 1/18,000?
This is possible by connecting one 1/180 gearhead with two 1/10 intermediate (decimal) gearheads. However, the allowable torque is the same as when using only a 1/180 gearhead. Note that the mounting screws included with the intermediate (decimal) gearheads are not long enough to connect two or more intermediate (decimal) gearheads, so you will need to prepare longer screws separately.