Can I use capacitors other than the one that comes with the AC motor?

As a general rule, use the capacitor that comes with the product.
However, if you need to use an emergency measure in the event that the capacitor is lost, use a non-polarized film capacitor for motors that has the same capacity and rated voltage as the included capacitor.

The capacitors included with the product are important components that allow the product to perform as specified.
Incorrect capacitance can cause torque loss, rotational vibration, overheating, etc.
Incorrect rated voltage can damage the capacitor, leading to smoke and fire, so please be careful.