- FAQ / KnowledgeBase
- αSTEP Step-Servo
For the AR series pulse train input type, what are the conditions for the END output to turn ON (the positioning complete signal to be output)?
The END output turns ON when the rotor is within ±1.8° of the command position with no pulse signal being input.
* When the pulse signal input frequency is 500Hz or less, the END output may turn ON irregularly.