---
title: I am using Modbus RTU control on the AR series with built-in positioning function. After turning the START input bit ON and running the controller, do I need to turn it OFF?
description: After turning the START input bit ON and operating, it must be turned OFF. A positioning operation is executed when the START input bit in the driver input command of the operation command changes fro
---

[Skip to content](https://faq.orientalmotor.com/i-am-using-modbus-rtu-control-on-the-ar-series-with-built-in-positioning-function.-after-turning-the-start-input-bit-on-and-running-the-controller-do-i-need-to-turn-it-off#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/?hsLang=en)
2. [Networking](https://faq.orientalmotor.com/networking?hsLang=en)

# I am using Modbus RTU control on the AR series with built-in positioning function. After turning the START input bit ON and running the controller, do I need to turn it OFF?

After turning the START input bit ON and operating, it must be turned OFF.

A positioning operation is executed when the START input bit in the driver input command of the operation command changes from 0 (OFF) to 1 (ON). To execute the next positioning operation, the START input bit must also change from 0 (OFF) to 1 (ON).

Therefore, the START input bit must be set to 0 (OFF) before executing the next positioning operation or any other operation.

Operation command - Driver input command

![AR\_remoteIO](https://faq.orientalmotor.com/hs-fs/hubfs/AR_remoteIO.png?width=688&height=160&name=AR_remoteIO.png)See the timing chart below for the timing at which the START input bit is set to 0 (OFF).

Driving Instructions

① Verify that the READY output is ON.

② Select the operation data number with the M0 to M5 inputs and turn the START input ON.

③ The motor starts positioning operation.

④ Verify that the READY output is OFF, then turn the START input OFF.

⑤ When the positioning operation is completed, the READY output turns ON.

![AR\_timing2](https://faq.orientalmotor.com/hs-fs/hubfs/AR_timing2.png?width=688&height=351&name=AR_timing2.png)

![AR\_timing](https://faq.orientalmotor.com/hs-fs/hubfs/AR_timing.png?width=688&height=468&name=AR_timing.png)

 

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo?hsLang=en)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors?hsLang=en)
- [Variable Speed / Brushless DC Motors](https://faq.orientalmotor.com/variable-speed-brushless-dc-motors?hsLang=en)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators?hsLang=en)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors?hsLang=en)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots?hsLang=en)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans?hsLang=en)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers?hsLang=en)
- [Software](https://faq.orientalmotor.com/software?hsLang=en)
- [Networking](https://faq.orientalmotor.com/networking?hsLang=en)
- [General](https://faq.orientalmotor.com/general?hsLang=en)
- [Servo](https://faq.orientalmotor.com/servo?hsLang=en)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom?hsLang=en)

- Home
- Products
- Pricing
- Blog
- Company

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.