---
title: For the AZ Series with built-in positioning function, is it possible to use FA network control and direct input/output at the same time?
description: Remote I/O via FA network control or Modbus communication and direct I/O can be used together. When the same input signal is assigned to remote I/O and direct I/O, the function will be executed if eit
---

[Skip to content](https://faq.orientalmotor.com/for-the-az-series-with-built-in-positioning-function-is-it-possible-to-use-fa-network-control-and-direct-input/output-at-the-same-time#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/?hsLang=en)
2. [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers?hsLang=en)

# For the AZ Series with built-in positioning function, is it possible to use FA network control and direct input/output at the same time?

Remote I/O via FA network control or Modbus communication and direct I/O can be used together.

When the same input signal is assigned to remote I/O and direct I/O, the function will be executed if either input is present.

The C-ON input \*1 and HMI input \*2 are always ON when not assigned to an input terminal.

Also, when assigned to both remote I/O and direct I/O, they will not function unless both are ON.

\*1 C-ON input

When it is turned ON, the motor is excited.

\*2 HMI input

When set to ON, the function restrictions of the support software MEXE02 are lifted.

 

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo?hsLang=en)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors?hsLang=en)
- [Variable Speed Motors](https://faq.orientalmotor.com/variable-speed-motors?hsLang=en)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators?hsLang=en)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors?hsLang=en)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots?hsLang=en)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans?hsLang=en)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers?hsLang=en)
- [Software](https://faq.orientalmotor.com/software?hsLang=en)
- [Networking](https://faq.orientalmotor.com/networking?hsLang=en)
- [General](https://faq.orientalmotor.com/general?hsLang=en)
- [Servo](https://faq.orientalmotor.com/servo?hsLang=en)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom?hsLang=en)

- Home
- Products
- Pricing
- Blog
- Company

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.