Is it okay to post-process the motor shaft?
Shaft processing after purchase
It is crucial that you refrain from any post-processing activities, as these actions could potentially harm the ball bearings and encoder within the motor. Additionally, it is imperative that you do not attempt to disassemble the motor under any circumstances. Disassembly can lead to a significant decline in performance and may result in the motor ceasing to rotate entirely.
If the application requires a customized shaft, it is recommended to contact our Technical Sales team for further evaluation.