Networking
- Do you offer PLC setup files/manuals?
- I'm rewriting parameters through communication (CC-Link network converter NETC01-CC to AZ), but when I turn the power back on, the parameters I thought I had changed disappear. Why is that?
- I am using Modbus RTU control on the AR series with built-in positioning function. After turning the START input bit ON and running the controller, do I need to turn it OFF?
- When data is written using the αSTEP AZ Drivers with Ethernet/IP communication, my changes are not saved in the drive and reverted back to the previous settings after a power cycle. How do I fix this?