αSTEP Step-Servo
AlphaStep Hybrid Step-Servo Motors
- What type of encoder is used on the AZ series step-servo hybrid motors?
- What type of encoder is used on the AZ series?
- For the AR/AZ series pulse train input type, how many pulses are output per rotation of the motor output shaft for the A-phase pulse output (ASG) and B-phase pulse output (BSG)?
- How much deviation is required to output an excessive position deviation alarm?
- The rotation speed units in the catalog are listed as two types, [Hz] and [r/min]. What is the difference between them?
- For the AR series pulse train input type, what are the conditions for the END output to turn ON (the positioning complete signal to be output)?
- I am using an αSTEP AZ EtherNet/IP compatible driver. Is direct I/O wiring required?
- I want to use the AZ series only on positive coordinates. How do I set this?