Controllers / Drivers
- What kind of PLC communication protocols does Oriental Motor offer?
- For the AZ Series with built-in positioning function, is it possible to use FA network control and direct input/output at the same time?
- How many milliseconds is the communication cycle of the AZ Series EtherNet/IP compatible driver?
- I am using the AZ series EtherNet/IP compatible driver. The fixed I/O signal EXE-ERR is ON. What kind of signal is EXE-ERR?
- Can I use 1 EMC filter in the input power supply connection for multiple drivers/controllers?