Software
- When I use the support software MEXE02 to operate the AZ series ZHOME, the message "Operation startup restriction mode" appears. What does this mean?
- I have multiple network-controllable products connected to the same master. If I connect the MEXE02 to the first unit, can I set data, teach, and remotely operate the units other than the first one?
- What happens if an external signal is input while performing teaching/remote operation with the MEXE02 or JOG operation with the OPX-2A?
- I am using an EtherNet/IP compatible driver for the AZ series. Is it possible to monitor data sent from a higher level using the support software MEXE02?