Skip to content
  • There are no suggestions because the search field is empty.

When I use the support software MEXE02 to operate the AZ series ZHOME, the message "Operation startup restriction mode" appears. What does this mean?

"Operation startup restriction mode" is information that occurs when commands cannot be accepted from the outside (direct I/O, network I/O).


The "Operation startup restriction mode" information will be generated not only during ZHOME operation, but also when "Teaching/Remote Operation" is being performed from the MEXE02 or when "Configuration" is being executed.