Skip to content
  • There are no suggestions because the search field is empty.

What is the difference between payload and thrust?

The payload is the weight that can be moved according to the specifications of the electric actuator.

Values ​​are set for both horizontal and vertical directions.


Thrust is the driving force that an electric actuator can use to push a load when speed is constant.

It is the force that acts on a moving load.