Skip to content
  • There are no suggestions because the search field is empty.

What happens when you use the "FREE" control on the MRC studio?

The "FREE" input deactivates the current supplied from the robot controller to the motors on the OVR. It is essential to exercise caution, as the robot may fall if it is not adequately supported after the FREE input is activated. .