Skip to content
  • There are no suggestions because the search field is empty.

What happens if an external signal is input while performing teaching/remote operation with the MEXE02 or JOG operation with the OPX-2A?

Operation command input signals (CW, CCW, START, FWD, RVS, etc.) are invalid.

Input signals other than operation commands (FREE, STOP, etc.) are valid.


Please see the table below for details on each series.

Input_signals

 

*The signals listed are only a part of the list.

For signals and products not listed in the table, please contact our technical support group