What happens if acceleration/deceleration is not controlled with a servo motor?
Although it depends on the magnitude of the load torque and the load moment of inertia, overshoot and undershoot will occur. If the overshoot and undershoot are large, it may have a negative effect (large vibration, large noise, etc.) on the workpiece and the customer's equipment. Please perform acceleration and deceleration control so that overshoot and undershoot are as small as possible.