Skip to content
  • There are no suggestions because the search field is empty.

What is the automatic current cutback function of stepping motor drivers?

The automatic current cutback function plays a crucial role in minimizing heat generation by decreasing the current supplied to the motor when it is not in operation. This function is triggered if the pulse signal remains inactive for a duration of 0.1 seconds or longer, ensuring efficient energy management and prolonging the lifespan of the motor.

This function is availabe in our stepper motor drivers like AZ series, AR series, CVD series, CRK series, RBK series and RK2 series.