Is there a way to reduce vibration during rotation?
Reducing Motor Vibration
There are four ways to reduce vibration during rotation:
(1) Use of microstep drive products
- AR Series
- AZ Series
- RKII series (with smooth drive function* )
- CRK series (with smooth drive function* )
- CVD series (with smooth drive function* )
(2) Use of clean dampers:
Vibrations are absorbed by the internal inertia mass and silicone gel.
(3) Vibration can be reduced by reducing the operating current adjustment torque.
(4) The use of geared motors reduces the transmission of vibration.
- *The smooth drive function
Is a function that performs microstep drive inside the driver while keeping the input pulse frequency and resolution unchanged, enabling low speed, low vibration, and low noise.