Skip to content
  • There are no suggestions because the search field is empty.

Is the surge suppression CR circuit "EPCR1201-2" shown in the wiring diagram of the circuit product necessary?

There is no problem with the operation of the circuit product even if you do not use a surge suppression CR circuit, but considering the lifespan of the relay contacts, we recommend using one. The surge suppression circuit suppresses sparks that occur when the relay contacts are turned on and off, and extends the lifespan of the relay contacts.