I would like to change the wiring of the blower so that the suction port and discharge port are reversed. Is this possible?
No. Even if you change the wiring, the suction port and discharge port will not change.
The relationship between the air in and out is determined not only by the rotation direction of the runner but also by the inclination angle of the runner's blades, so both the air volume and static pressure will decrease.