Skip to content
  • There are no suggestions because the search field is empty.

I want to use the AZ series only on positive coordinates. How do I set this?

AZ Series Wrap Settings

Setting the "Initial coordinate generation & wrap range offset ratio" in the "Motor & mechanism (Coordinates/JOG/Home) settings" parameter to 0.00% restricts usage to positive coordinates exclusively.

Wrap_setting