Skip to content
  • There are no suggestions because the search field is empty.

I have multiple network-controllable products connected to the same master. If I connect the MEXE02 to the first unit, can I set data, teach, and remotely operate the units other than the first one?

When connecting a driver to the MEXE02 software, it is only possible to set data and perform teaching and remote operation for the unit connected to it.