I am using the DSC series and an alarm code beginning with AL is displayed on the front panel of the speed controller. What is the meaning of this alarm code?
The alarm code is displayed when a protective function is activated and an alarm occurs.
Check the alarm content from the corresponding alarm code below.
For details, please refer to the DSC series instruction manual .
✅