Skip to content
  • There are no suggestions because the search field is empty.

I am using a motor with a load attached directly to the output shaft facing upwards. What should I be careful of in this case?

Axial Load

The axial (thrust) load resulting from the applied force significantly impacts the lifespan of the bearing. It is essential to ensure that this load remains within the specified allowable limits. When the axial load exceeds these limits, it can hinder proper preloading of the bearing, potentially leading to fatigue wear over time. For detailed information on the allowable axial load, please consult the catalog.

Incorporating a gearhead with the motor can enhance the axial load handling capabilities.