Skip to content
  • There are no suggestions because the search field is empty.

What motion commands are supported in the MRC Studio software?

Motions types are the specific movements one can do within the MRC Studio software

The MRC software supports a total of 13 distinct motion types.
  • PTP (Point-to-Point)
  • Linear Movement
  • Circular Motion (Clockwise)
  • Circular Motion (Counterclockwise)
  • Circular Motion via Point
  • Arch Motion
  • Axis Movement
  • End Effector 1
  • End Effector 2
  • Return to Origin
  • Pallet Point-to-Point
  • Pallet Linear Motion
  • Pallet Arch Motion
mrcu-lm-feature-easy-setup-2