How many milliseconds is the communication cycle of the AZ Series EtherNet/IP compatible driver?
It can be set between 1 [ms] and 3,200 [ms].
To change the communication cycle, use the setting tool of the scanner (host system).
* The communication cycle setting cannot be changed using our support software MEXE02.
Communication diagram of Implicit message (when communication cycle is 10 ms)