---
title: Software | FAQ / KnowledgeBase
description: Software
---

[Skip to content](https://faq.orientalmotor.com/software#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/)
2. [Software](https://faq.orientalmotor.com/software)

# Software

- [When I use the support software MEXE02 to operate the AZ series ZHOME, the message "Operation startup restriction mode" appears. What does this mean?](https://faq.orientalmotor.com/when-i-use-the-support-software-mexe02-to-operate-the-az-series-zhome-the-message-operation-startup-restriction-mode-appears.-what-does-this-mean)
- [I have multiple network-controllable products connected to the same master. If I connect the MEXE02 to the first unit, can I set data, teach, and remotely operate the units other than the first one?](https://faq.orientalmotor.com/i-have-multiple-network-controllable-products-connected-to-the-same-master.-if-i-connect-the-support-software-mexe02-to-the-first-unit-can-i-set-data-teach-and-r-1727277089838)
- [What happens if an external signal is input while performing teaching/remote operation with the MEXE02 or JOG operation with the OPX-2A?](https://faq.orientalmotor.com/what-happens-if-an-external-signal-is-input-while-performing-teaching/remote-operation-or-remote-operation-with-the-mexe02-or-jog-operation-with-the-opx-2a)
- [I am using an EtherNet/IP compatible driver for the AZ series. Is it possible to monitor data sent from a higher level using the support software MEXE02?](https://faq.orientalmotor.com/i-am-using-an-ethernet/ip-compatible-driver-for-the-az-series.-is-it-possible-to-monitor-data-sent-from-a-higher-level-using-the-support-software-mexe02)
- [Can I use the Ethernet IP driver EDS/AOI files with RS Logix?](https://faq.orientalmotor.com/can-i-use-the-ethernet-ip-driver-eds/aoi-files-with-rs-logix)

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors)
- [Variable Speed Motors](https://faq.orientalmotor.com/variable-speed-motors)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers)
- [Software](https://faq.orientalmotor.com/software)
- [Networking](https://faq.orientalmotor.com/networking)
- [General](https://faq.orientalmotor.com/general)
- [Servo](https://faq.orientalmotor.com/servo)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom)

- Home
- Products
- Pricing
- Blog
- Company

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.