---
title: Industrial Robots | FAQ / KnowledgeBase
description: Industrial Robots
---

[Skip to content](https://faq.orientalmotor.com/industrial-robots#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/)
2. [Industrial Robots](https://faq.orientalmotor.com/industrial-robots)

# Industrial Robots

- [How do I Check for theTCP position limit of my OVR robot vias the MRC studio software .](https://faq.orientalmotor.com/how-do-i-check-for-thetcp-position-limit)
- [How do I check the origin of my OVR robot Via the MRC Studio software ?](https://faq.orientalmotor.com/how-do-i-check-the-origin-of-my-ovr-robot-)
- [How do I set the position limit on the MRC Studio Software](https://faq.orientalmotor.com/how-do-i-set-the-position-limit-)
- [What is the Definition of right-handed system / left-handed systems in SCARA and 6 Axis robots?](https://faq.orientalmotor.com/what-is-the-definition-of-right-handed-system-/-left-handed-system-in-scara-robots-mean-)
- [What the Coordinate system the OVR robots can work with ?](https://faq.orientalmotor.com/what-the-coordinate-system-the-ovr-robots-can-work-with-)
- [How many degrees of freedoms are present for each robot type ?](https://faq.orientalmotor.com/are-there-any-inspection-and-maintenance-that-needs-to-be-doen-with-the-mrc-)
- [Is the MRC01 and the MRC01-C the same controller ?](https://faq.orientalmotor.com/is-the-mrc01-and-the-mrc01-c-the-same-controller-)
- [What are the I/O signals cables that are offered for the MRCU controllers ?](https://faq.orientalmotor.com/what-are-the-i/o-signals-cables-that-are-offered-for-the-mrcu-controllers-)
- [What connection cables / flexible connection cables are offered for the OVR motors ?](https://faq.orientalmotor.com/what-connection-cables-/-flexible-connection-cables-are-offered-for-the-ovr-motors-)
- [What is the power supply cable for the MRCU Robot controller and there pin out ?](https://faq.orientalmotor.com/what-is-the-power-supply-cable-for-the-mrcu-robot-controller-and-there-pin-out-)
- [Does the MRCU controller need any maintenance ?](https://faq.orientalmotor.com/does-the-mrcu-controller-need-any-maintenance-)
- [How do you set up the MRC Studio Software?](https://faq.orientalmotor.com/how-do-you-set-up-the-mrc-studio-software-)
- [For the MRCU and OVR robots, are there any noise suppression tips we can use ?](https://faq.orientalmotor.com/for-the-mrcu-and-ovr-robots-are-there-any-noise-suppressions-tips-we-can-use-)
- [For the MRCU and OVR robots are there any prevention of noise propagation tips we can use ?](https://faq.orientalmotor.com/for-the-mrcu-and-ovr-robots-are-there-any-prevention-of-noise-propagation-tips-we-can-use-)
- [What is the main power supply current capacity for the MRCU controller?](https://faq.orientalmotor.com/what-are-the-current-capacities-for-the-main-power-supply-)
- [What do the LEDs on the MRCU controllers mean?](https://faq.orientalmotor.com/what-are-the-leds-on-the-mrcu-controllers-mean-)
- [What is the Current Capacity for Control Power Supply on the MRCU ?](https://faq.orientalmotor.com/what-is-the-current-capacity-for-control-power-supply-on-the-mrcu-)
- [Is there a information that can be stored on the MRCU and then shared via the I/O](https://faq.orientalmotor.com/is-there-a-information-that-can-be-stored-on-the-mrcu-and-then-shared-via-the-i/o-)
- [Is the MRCU controller equipped with a function to generate information output before an alarm ca be generated?](https://faq.orientalmotor.com/is-the-mrcu-controller-equipped-with-a-function-to-generate-information-output-before-an-alarm-ca-be-generated)
- [Can you check the Alarm History on the MRCU controller ?](https://faq.orientalmotor.com/can-you-check-the-alarm-history-on-the-mrcu-controller-)
- [Can you reset the Alarms on the MRCU ?](https://faq.orientalmotor.com/can-you-reset-the-alarms-on-the-mrcu-)
- [What are the Voltage specifications for the MRCU controller ?](https://faq.orientalmotor.com/what-are-the-voltage-specifications-for-the-mrc-controller-)
- [Are there any alarm function that the OVR  systems have ?](https://faq.orientalmotor.com/are-there-any-alarm-function-that-the-ovr-systems-have-)
- [What is the payload amount for the OVR series 4-Axis Articulated Robot?](https://faq.orientalmotor.com/what-is-the-payload-amount-for-4-axis-articulate-robot)
- [Do you offer a programming software for the OVR Robots?](https://faq.orientalmotor.com/do-you-offer-software-for-the-use-of-you-ovr-systems)
- [What type of end effectors does Oriental Motor offer for OVR Robots?](https://faq.orientalmotor.com/what-are-end-effectors-that-we-offer-for-our-ovr-machine)
- [What is the payload amount for the 5-Axis Articulated Robot?](https://faq.orientalmotor.com/what-is-the-payload-amount-for-4-axis-articulate-robot-1)
- [What is the payload amount for the 6-Axis Articulated Robot?](https://faq.orientalmotor.com/what-is-the-payload-amount-for-4-axis-articulate-robot-2)
- [What is the payload amount for the 3-Axis SCARA Robot?](https://faq.orientalmotor.com/what-is-the-payload-amount-for-scara-robot)
- [What is the payload amount for the 3-Axis Cartesian Robot?](https://faq.orientalmotor.com/what-is-the-payload-amount-for-3-axis-gantry-systems)
- [Do you offer industrial robots?](https://faq.orientalmotor.com/do-you-offer-robots)
- [What are the significant specs for the OVR Series Cartesian 3-Axis robot ?](https://faq.orientalmotor.com/fhdzhfj)
- [What are the significant specs for the OVR series SCARA robot ?](https://faq.orientalmotor.com/what-are-the-significant-specs-for-the-scara-ovr-robot)
- [What are the significant specs for the 4-Axis OVR series robot ?](https://faq.orientalmotor.com/what-are-the-significant-specs-for-the-4-axis-ovr-robot)
- [What are the significant specs for the 5-axis OVR series robot ?](https://faq.orientalmotor.com/what-are-the-significant-specs-for-the-5-axis-ovr-robot)
- [What are the significant specs for the 6-Axis OVR series robot ?](https://faq.orientalmotor.com/what-are-the-significant-specs-for-the-6-axis-ovr-robot)
- [What motion commands are supported in the MRC Studio software?](https://faq.orientalmotor.com/how-many-motions-types-are-there-in-the-software)
- [What are some application we can use the OVR series robots systems in?](https://faq.orientalmotor.com/what-are-some-application-we-can-use-the-ovr-robots-systems-in)
- [What happens when you use the "FREE" control on the MRC studio?](https://faq.orientalmotor.com/what-happens-when-you-use-the-free-control)
- [What are the control methods of the MRC01 Robot Controller ?](https://faq.orientalmotor.com/what-are-the-control-methods-of-the-mrc)
- [Can I use a third party end effector with Oriental Motor OVR series Robot?](https://faq.orientalmotor.com/can-you-use-a-third-party-end-effector-with-oriental-motor-ovr)
- [Why can I not see the Simulator Software Program MRCXT file open ?](https://faq.orientalmotor.com/why-can-i-not-see-the-simulator-software-program-mrcxt-file-open)
- [How many control commands are there in the MRC Studio software?](https://faq.orientalmotor.com/how-many-control-types-are-there-in-the-software)
- [Electric Robotic arms vs Pneumatic Robotic Arms](https://faq.orientalmotor.com/electric-robotic-arms-vs-pneumatic-robotic-arms)
- [Can you mount the OVR on a vertical wall?](https://faq.orientalmotor.com/can-you-mount-the-ovr-on-vertical-wall)
- [What are the Installation Location Recommendation for the OVR and MRC Products?](https://faq.orientalmotor.com/what-are-the-installation-location-recommendation-for-the-ovr-and-mrc-products)
- [For the MRCU is there any concerns for Surge Suppressors ?](https://faq.orientalmotor.com/for-the-mrcu-is-there-any-concerns-for-surge-suppressors-)
- [How Does one set up the Robot on the MRC Studio?](https://faq.orientalmotor.com/how-does-one-set-up-the-robot-on-the-mrc-studio)
- [How do I set the Origin of my robot Through  the MRC Software ?](https://faq.orientalmotor.com/how-do-i-set-)

See less ▼

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors)
- [Variable Speed / Brushless DC Motors](https://faq.orientalmotor.com/variable-speed-brushless-dc-motors)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers)
- [Software](https://faq.orientalmotor.com/software)
- [Networking](https://faq.orientalmotor.com/networking)
- [General](https://faq.orientalmotor.com/general)
- [Servo](https://faq.orientalmotor.com/servo)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom)

- Home
- Products
- Pricing
- Blog
- Company

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.