---
title: I'm concerned about the heat (surface temperature) of stepping motors (including αSTEP). Is this abnormal?
description: It can be used if the motor case surface temperature is 100°C or less. The motor's insulation class is Class B insulation, with an allowable temperature of 130°C for the windings. Since there is an ex
---

[Skip to content](https://faq.orientalmotor.com/im-concerned-about-the-heat-surface-temperature-of-stepping-motors-including-αstep.-is-this-abnormal#main-content)

![Oriental Motor U.S.A. Corp.](https://faq.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?height=40&name=OM-logo-200px.jpg)

Open main navigation

Close main navigation

- [Go to orientalmotor.com](https://www.orientalmotor.com/)

[Go to orientalmotor.com](https://www.orientalmotor.com/)

 Hello. How can we help you?

- There are no suggestions because the search field is empty.

1. [FAQ / KnowledgeBase](https://faq.orientalmotor.com/?hsLang=en)
2. [Stepper Motors](https://faq.orientalmotor.com/stepper-motors?hsLang=en)

# I'm concerned about the heat (surface temperature) of stepping motors (including αSTEP). Is this abnormal?

It can be used if the motor case surface temperature is 100°C or less.

The motor's insulation class is Class B insulation, with an allowable temperature of 130°C for the windings. Since there is an expected temperature difference of 30°C between the inside of the motor and the case surface, the upper limit on the case surface is 100°C.

Use the AZ series at a motor case surface temperature of 80°C or less. If the ABZO sensor temperature reaches 85°C or higher, a motor overheat protection alarm will occur.

Consider the lifespan of the motor's ball bearings, attach them to a metal plate with good thermal conductivity, and use them at the lowest possible temperature. The bearings have a lifespan of 50,000 hours when the motor case surface temperature is 80°C. If used at temperatures above 80°C, the motor's lifespan will be shortened.

The UL/CSA certification requirement is Class A insulation (105°C). When applying for a set as a UL/CSA certified product, please use the motor at a surface temperature of 75°C or less.

If you are concerned about the surface temperature of your stepping motor, there are ways to prevent the temperature from increasing.  

- [αSTEP Step-Servo](https://faq.orientalmotor.com/%CE%B1step-step-servo?hsLang=en)
- [Stepper Motors](https://faq.orientalmotor.com/stepper-motors?hsLang=en)
- [Variable Speed Motors](https://faq.orientalmotor.com/variable-speed-motors?hsLang=en)
- [Linear / Rotary Actuators](https://faq.orientalmotor.com/linear-rotary-actuators?hsLang=en)
- [AC Gearmotors](https://faq.orientalmotor.com/ac-gearmotors?hsLang=en)
- [Industrial Robots](https://faq.orientalmotor.com/industrial-robots?hsLang=en)
- [Cooling Fans](https://faq.orientalmotor.com/cooling-fans?hsLang=en)
- [Controllers / Drivers](https://faq.orientalmotor.com/controllers-drivers?hsLang=en)
- [Software](https://faq.orientalmotor.com/software?hsLang=en)
- [Networking](https://faq.orientalmotor.com/networking?hsLang=en)
- [General](https://faq.orientalmotor.com/general?hsLang=en)
- [Servo](https://faq.orientalmotor.com/servo?hsLang=en)
- [Cleanroom](https://faq.orientalmotor.com/cleanroom?hsLang=en)

- Home
- Products
- Pricing
- Blog
- Company

[![www.orientalmotor.comimagesmainTopOM-logo-200px](https://faq.orientalmotor.com/hs-fs/hubfs/social-suggested-images/www.orientalmotor.comimagesmainTopOM-logo-200px.jpg?width=200&height=47&name=www.orientalmotor.comimagesmainTopOM-logo-200px.jpg "www.orientalmotor.comimagesmainTopOM-logo-200px")](http://www.orientalmotor.com)

FAQ / KnowledgeBase

Copyright © 2025, ORIENTAL MOTOR USA Corp.